Cancel
Showing results for 
Search instead for 
Did you mean: 

Managing memory during an rms solve (Nx10)

Gears Phenom Gears Phenom
Gears Phenom

To all I have a small programme which does the following;

For every groups and every resp. sim events selected

  1. Predict rms forces

   2. Write data to xls (.csv)

 

Once all processed, combined the xls file created

Programme does the job.

 

What I have noticed is that NX.10 is using a huge amount of memory and not releasing it on completion of the task.

 

Just did a test with 190 elements, 3 events, and according to the task manager, the Physical Memory graph is showing ~85Gb used (that’s half of what is available) and it’s staying there. I need close Nx to release it.

 

Is there anyway of flushing this memory during the programme? In another test I used 6 events (190elms) and the machine run out of memory!

 

Thanks

Regards

Production: NX.CAE 9.0.3.4, NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)