Cancel
Showing results for 
Search instead for 
Did you mean: 

Material attributes

Gears Phenom Gears Phenom
Gears Phenom

Setting up NX11, and I saw in the help files, about the "NX Title for system attributes" changing.  So I started to look at the Customer Default settings.....we have both object, and part material attributes.  When you assign a material in NX, if the file only has one body, I assume that gives the material value to both the Part, and the Object.  If you have multiple bodies, you could have different materials assigned to different 'objects'.  If I am pushing the material value to Teamcenter, and the drawing, this would be the "Part Material"?

-Dave
NX 11 | Teamcenter 11 | Windows 8.1