Cancel
Showing results for 
Search instead for 
Did you mean: 

Maximum possible number of entries in Integer or double table in block UI styler in NX9?

Pioneer
Pioneer

Hi All,

How many entries can one give in doubles or integer table.

I want to give 5000 entries. Is this possible to give that much of entries??

 

Thanks 

 

3 REPLIES

Re: Maximum possible number of entries in Integer or double table in block UI styler in NX9?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I think this is a huge number of entries, which will make the dialog look really bad.

 

How about using a grid control instead (don't know if it is called grid in NX).

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Maximum possible number of entries in Integer or double table in block UI styler in NX9?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Or use Excel (embedded or external)

And if external, you oculd read from the XLS[x] file or save as comma/tab separated text.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Maximum possible number of entries in Integer or double table in block UI styler in NX9?

Phenom
Phenom

Just for fun I had a go at this. Creating a DoubleTable with 500 rows and a single column took about 7 seconds to construct the dialog. When I tried 5000 rows and a single column I got

"Internal Error - Memory Access Violation".

Had to kill NX using the task manager.

Note this was using NX8.5 but I suspect the same would happen in NX9.

Graham Inchley Snr R&D Engineer (Systems Development), Sandvik Coromant
Lenovo ThinkPad W540, Win7, 16GB. Developing in: Java | C | KF
Production: [NX8.5.3.3 MP11 64bit] Testing: [NX12.0.0.27 MP1]