Cancel
Showing results for 
Search instead for 
Did you mean: 

Memory Access Violation

Innovator
Innovator

I realize this is will be very vague, but there are times when I go to make a feature the current feature by calling the "Feature.MakeCurrentFeature()".

And it would give me a memory access violation.

Any ideas?

1 REPLY

Re: Memory Access Violation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Try doing it intercactively & see if you get a better error message.

If this is all buried in code, "catch" the error, output a message saying which feature you are using, and exit your API code, then try to do it interactively.

 

Have you looked into the syslog (menu location depends on NX version, but it is something like "Help" -> "NX log file"

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled