Cancel
Showing results for 
Search instead for 
Did you mean: 

Memory issue

Innovator
Innovator

We have a program that is copying and pasting a set of features from a part.

The problem is that even though the program is completing properly and we are calling the appropriate CopyPasteBuilder2.Destroy methods. Our Ram is going up every time we run the program.

And it doesn't go down until we end the current session of NX.

Any idea or somthing else I should be calling would be greatly appreciated. Thank you.

1 REPLY

Re: Memory issue

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You probably need to report this to GTAC.

 

Does it do the same thing (consume RAM) when you copy/paste interactively?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled