Cancel
Showing results for 
Search instead for 
Did you mean: 

Modify Journal code to rename parts

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

I found one journal which renames the component names in the assembly navigator. I tried the following scenario.

 

1) When assembly is exported as JT, all parts are getting suffix "_jt" in their name.

 

Jt.PNG

 When I run the journal it removes suffix _jt from all parts.

 

jt1.PNG

 

 2) Now when assembly is exported as parasolid. Components gets suffix as _id6_x_t, _id11_x_t etc.

jt2.PNG

 

What I understood is line in journal to rename parts is

 

Dim newShortName As String = oldShortName.Replace("_jt", "")

If I modify this as

 

Dim newShortName As String = oldShortName.Replace("_id6_x_t", "")

 

It will only rename one component. If I want to rename the all components by removing respective suffix _id6_x_t, _id11_x_t etc. Is this possible to modify code in such way? If yes. It would be nice to have code with modification. I dont know whether it is possible or not, I am not the person having coding knowledge. Smiley Happy

 

 

4 REPLIES

Re: Modify Journal code to rename parts

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Using regular expression pattern matching is one way to find the "_idn_x_t" suffix in each part. However, if we remove the suffix, each part in your example assembly would end up with the same name. I see no safeguards in the journal code to avoid overwriting an existing file; so the code would save a part, then overwrite it when the next one gets saved. The result would be one component part in your directory, whichever happened to be saved last; the rest of the files would be lost.

Re: Modify Journal code to rename parts

Siemens Phenom Siemens Phenom
Siemens Phenom

Exporting the assembly as parasolid we need to provide the name and all the components of parasolid gets the same name with suffix like _id1_x_t, _id2_x_t etc. So is it ok to conclude that there is no way retain the name of components in parasolid like it is possible when exporting the assembly using the STEP format.

Re: Modify Journal code to rename parts

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Re: Modify Journal code to rename parts

Siemens Phenom Siemens Phenom
Siemens Phenom

Thank you @cowski1 Smiley Happy