Cancel
Showing results for 
Search instead for 
Did you mean: 

Moving a Non associative point using moveobject Feature in NX

Creator
Creator

I had created a Tube through programming using C++ lang, Using two Non-Associative point & line, I am trying to move that non-associative object using MoveObject Feature of NX, But i am not able to do so, it is displaying that a fixed point will get created because the Point "Output Co-ordinate Reference" is set to "WCS" & then i had set it to "Absolute WorkPart" but still the results are same.

 

Do any have an idea how i can move a non-associative point or an alternate solution for it.

Thanks in advance.

3 REPLIES

Re: Moving a Non associative point using moveobject Feature in NX

Phenom
Phenom

Have you tried Edit -> Transform to move the point?

Suresh

Re: Moving a Non associative point using moveobject Feature in NX

Creator
Creator

I tried it with Edit->Transform , but it is making a copy of a point & not able move that non-associative point as well as Tube Feature is not getting Updated w.r.t to copied point.

I want to move that point with help MoveObject Feature as it's is requirement.

Do you know ,how can i handle the Refrence CSYS from not setting it to WCS as it is creating a fixed point. 

 

Thanks in advance for your valuable time.

 

Re: Moving a Non associative point using moveobject Feature in NX

Phenom
Phenom

The code snippet below creates two non associative points and an associative line between them.  I can move the points around and the line updates.

 

	Point3d stPoint(10.0, 10.0, 0);
	Point3d endPoint(10.0, 100.0, 0);
	Point *point1 = workPart->Points()->CreatePoint(stPoint);
	Point *point2 = workPart->Points()->CreatePoint(endPoint);
	Line *line1 = workPart->Curves()->CreateLine(point1, point2);
	point1->SetVisibility(SmartObject::VisibilityOptionVisible);
	point2->SetVisibility(SmartObject::VisibilityOptionVisible);
	line1->SetVisibility(SmartObject::VisibilityOptionVisible);
Suresh