Cancel
Showing results for 
Search instead for 
Did you mean: 

NVidia driver versions

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

NVidea graphics card driver versions...

How does one map from the version in the certification table & NVidea web site (e.g. 362.13) to the version reported in windows (under Device manager -> Display adapters -> NVidia Quadro Pro -> Properties -> Driver) which shows "21.21.13.6981" on my workstation?

 

 

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


2 REPLIES

Re: NVidia driver versions

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

After searching for hours....

NVidea control panel -> click on "Home" icon - it's right there...

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: NVidia driver versions

Legend
Legend

use the last 5 numbers

 

21.21.13.6981

 

So this is 369.81