Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 10 - Siemens Documentation Server - memory usage

Builder
Builder

Hello,

after instal NX10 and documentation, new documentation server has very high memory usage.

I have win 8.1 pro x64. Is this normal?

doc_server.jpg

6 REPLIES

Re: NX 10 - Siemens Documentation Server - memory usage

Siemens Phenom Siemens Phenom
Siemens Phenom

Yes, it is normal.

Re: NX 10 - Siemens Documentation Server - memory usage

Pioneer
Pioneer

For reference, not on Win8:

 

I installed it at my Win7 laptop, there it utilizes 940MB.

 

At the company site I deployed it to a JBOSS7.1 that one utilizes 1,7GB right now but I do not know how much memory was used before because that server has other tasks to do as well.

Thomas Zwatz, CADadmin, PÖTTINGER Landtechnik GmbH
Production: NX11.0.2.7 MP4 + TC10.1.7.1
Testing: NX11.0.2.7 MP4 + TC10.1.7.1
Development: C#

Re: NX 10 - Siemens Documentation Server - memory usage

Experimenter
Experimenter

Hello,

 

I have the same problem. But for me this memory consumption is not normal, it is too high. It is slowing down my computer and even preventing from calculation of complex toolpaths because of high memory demands.

 

Did anyone try to lower/limit somehow the memory consumption?

 

Thanks

with regards Jan Tomicek

Re: NX 10 - Siemens Documentation Server - memory usage

Valued Contributor
Valued Contributor

I found a document in the uganswer database:

By default the SPLM Documentation Server 1.0 has a large memory footprint on Windows. This will be reduced in later versions, but for the initial release this has to be manually configured. The large memory footprint is a result of the default Java heap size that is set during the installation process.  For a server that is used by a small number of users, these default values are too large resulting in an unnecessary large memory footprint.

 

Mit freundlichen Grüßen / With kind regards

i.A. Dipl.-Ing. (FH) Stefan Walder
CAD Management
----------------------------------------------------------------------
stefan.walder@gira.de
Tel +49(0)2195-602-319, Fax +49(0)2195-91603-319
----------------------------------------------------------------------
Gira Giersiepen GmbH & Co. KG, Elektro-Installations-Systeme
Industriegebiet Mermbach, Dahlienstraße, 42477 Radevormwald, Deutschland

Intelligente Gebäudetechnik von Gira. www.gira.de

Handelsregister AG Köln HRA 16352
Persönlich haftende Gesellschafterin: GAV Management GmbH,
Handelsregister AG Köln HRB 50479
Geschäftsführer: Dipl.-Kfm. Dirk Giersiepen, Alfred A. Bulitz,
Dipl.-Kfm. Thomas Musial
----------------------------------------------------------------------
Gira Giersiepen GmbH & Co. KG, Electrical installation systems
Industriegebiet Mermbach, Dahlienstraße, 42477 Radevormwald, Germany

Intelligent building technology by Gira. www.gira.com

Register of Business Names: AG Köln HRA 16352
Partner Personally Responsible: GAV Management GmbH,
Register of Business Names: AG Köln HRB 50479
Managing Directors: Dipl.-Kfm. Dirk Giersiepen,
Dipl.-Wirtschafts-Ing. (FH) Oliver Borchmann, Alfred A. Bulitz,
Dipl.-Kfm. Thomas Musial

Re: NX 10 - Siemens Documentation Server - memory usage

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Stefan,

 

You are correct, forgot to post the original link here as well. But well spotted Smiley Happy

 

If anyone is looking for the original document, look here:

https://solutions.industrysoftware.automation.siemens.com/docs/newsletter/splm-documentation-server-... (Webkey required)

 

Kind regards

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: NX 10 - Siemens Documentation Server - memory usage

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I had found that document a week ago looking for something else.

Anyway, I did some testing and on my system I was able to lower the values as per the image below and go the memory usage down to about 500Mb.

I did get the values to a point where it wasn't working at all, so I'm sticking with what's set below.

Also need to stop & restart the Doc service to pick up the new memory values.

 

2015-06-19_9-11-52.jpg

 

2015-06-19_9-12-31.jpg

Anthony Galante, Senior Support Engineer
PhoenxPLM
24 versions of NX installed: NX4 to NX12, plus TC11.2