Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 11 Python Making GUIs

Creator
Creator

Hello all,

 

I would like to ask what is the best way to go about making GUIs (graphical user interfaces) in NX. Does something like tkinter work on NX?

 

Let me know thanks!

5 REPLIES 5

Re: NX 11 Python Making GUIs

Siemens Phenom Siemens Phenom
Siemens Phenom

Re: NX 11 Python Making GUIs

Creator
Creator

 Thank you JimB!

Re: NX 11 Python Making GUIs

Experimenter
Experimenter

Does Block UI Styler output the template code in language other than C#?  My journal output is set to Python but I don't see an option to set the output for the Block UI Styler code.

Re: NX 11 Python Making GUIs

Siemens Phenom Siemens Phenom
Siemens Phenom
Block Styler can generate code in all the usual supported languages, including Python. The “Generate Code” function in Block Styler has a menu for choosing the output language. It’s completely independent from the language setting for recording journals.

I don’t know whether tkinter works or not. But, even if it does, it will be difficult to create a UI that looks and behaves like the rest of NX. Simple stuff might work OK, but implementing graphical selection of NX objects (for example) is going to be a major pain.
山田
yamada
Highlighted

Re: NX 11 Python Making GUIs

Genius
Genius

image.png