Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 9.0.3 Update

Genius
Genius

Was anyone able to download NX9.0.3 update successfully?

 

I have tried downloading that zipped file several times from work and from home with no luck.  The file downloads fine but when extracting it fails. 

 

Jerry

 

7 REPLIES

Re: NX 9.0.3 Update

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Worked fine and have it installed and running.

 

Have you already tried turning your AV software off before downloading?

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: NX 9.0.3 Update

Genius
Genius

Stefan,

Yes I did try that :-(

I downloaded the full version of 9.0 no problem as they did not send us DVDs anymore.  Just that latest update I cannot get it.  Like I said I even tried it from my home - different provider and different network and nothing helps.  Keeps failing about half way while extracting the files.

Jerry

 

Re: NX 9.0.3 Update

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Shooting in  the dark...

Did you compare file sizes (on GTAC vs on your PC)?

What software are you using to extract the files (IIRC there was a posing by GTAC that 7 Zip may work better than WinZip)?

You sure you have enough disk space to extract the files?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: NX 9.0.3 Update

Siemens Phenom Siemens Phenom
Siemens Phenom
  1. You are downloading nx-9.0.3.zip, correct?
  2. Have you verified the md5 checksum? It should be 084511b6e3b7d77bd6621018cd34cb15
  3. Same question/suggestion as Ken about the utility used to extract. I've successfully used both 7zip and Windows Explorer in Windows 7 Professional. If you are using something else, try one of those.

Re: NX 9.0.3 Update

Genius
Genius

This is what I get:

 

C:\>fciv c:\nx-9.0.3.zip

// File Checksum Integrity Verifier version 2.05.

084511b6e3b7d77bd6621018cd34cb15 c:\nx-9.0.3.zip

 

Then I try to unzip it with WinZip V12.1.

Same WinZip that I unzipped NX9.0.0 no problem.

 

Do you think I need something different than WinZip???

 

Re: NX 9.0.3 Update

Siemens Phenom Siemens Phenom
Siemens Phenom

Yes

Re: NX 9.0.3 Update

Genius
Genius

Extracting files using Windows Explorer works fine.  Using WinZip fails.

Thanks for help guys!

Jerry