Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 9 custom icon for carrier

Experimenter
Experimenter

Hello, everyone.

 

I got a small problem and need your help.

I need to replace a standart "carrier" icon in tool window. For my work i made a lot of tool templates, and for more user-friendly interface i need to replace that green (carrier) hexagon with an icon of that tooltype that lies inside.

I know that in older version(8.5) this is acceptable, so can i make it through in NX9?!

 

If you could show me where to look it will be awesome.

 

Thank you.

2 REPLIES 2

Re: NX 9 custom icon for carrier

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

This can be controlled with object attributes:

  • select the object
  • from the context menu select properties
  • open the attributes tab
  • change the CAM_ICON attribute

Hope this helps.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: NX 9 custom icon for carrier

Experimenter
Experimenter

It worked. thank you!