Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 9 will not start

Experimenter
Experimenter

I am running Win 7 and NX 9.0.2 and use the same install script for over 50 PCs but I have one that hangs on the ugraf process. I get the splash screen for a few seconds, then it goes away and the ugraf process is still running. Any Ideas?

5 REPLIES

Re: NX 9 will not start

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Look in the TMP folder for the syslog (username/gibberish/.syslog)

 

If ugraf.exe is still running, it could be the NX window is off the screen?

(did this user used to have a 2nd monitor or ???)

Get rid of

- C:\Users\kakerboo\AppData\Local\Siemens\NX90 folder

- similar files/folder if UGII_USER_DIR or other ENVs store files elsewhere

- Registry delete HKCU\Software\Unigraphics solutions\NX\9.0

 

(you may want to keep backups before you delete)

See if that pulls it up on-screen?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: NX 9 will not start

Experimenter
Experimenter

The process for ugraf.exe stalls at 100,824K on this PC and all the other installations ugraf.exe is using 155,240K. The syslog shows NX stops during or just after loading ugpcbxchange\startup\pcbm_app.mem.

 

I tried all the previous suggestions with no luck. I am totally stumped on this one

Re: NX 9 will not start

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Reinstallation already tried?

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: NX 9 will not start

Experimenter
Experimenter
uninstalled and reinstalled several times

Re: NX 9 will not start

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Have a look at your graphics driver.

 

\ugpcbxchange\startup\pcbm_app.men is loaded right before intialisation of the graphics driver for NX, so that's where I would be looking at why NX doesn't start.

 

Try to use the certified driver for your card, or the latest one available.

NX graphics certification

Anthony Galante, Senior Support Engineer
PhoenxPLM
24 versions of NX installed: NX4 to NX12, plus TC11.2