Cancel
Showing results for 
Search instead for 
Did you mean: 

NX Body to PLY File

Attached is a program that creates an PLYfile.  Because I use some linq commands it cannot be run as a journal.  I have included the vb code, the signed dll for NX or NX12 and a dialog file for selecting a body and defining the output file name.

 

Frank Swinkels

2 REPLIES 2

Re: NX Body to PLY File

Creator
Creator

how i can install it ???

Re: NX Body to PLY File

To use ExportPLYFile, simply put  PLYExportDialog.dlx into the 'application' subfolder of your customization folder which can be defined by different ways:

Either set the UGII_USER_DIR environment variable to point to the customization folder or add the full directory path of your customization folder to the file specified by UGII_CUSTOM_DIRECTORY_FILE which defaults to $(UGII_BASE_DIR)\ugii\menus\custom_dirs.dat.

 

Frank Swinkels