Cancel
Showing results for 
Search instead for 
Did you mean: 

NX Intellectual property logging mechanisms

Experimenter
Experimenter

Hello Friends,

I need help in the below requirement. One of our customer has 1000+ users working on NX 9.0.3.4 with TC 10.1.3.2 integration. Admin would like to track what data is exported or imported to and from desktop (like .prt to parasolid,stp etc.,) (NX Intellectual property logging mechanisms. We need a complete logging of what users import & export from/to NX like parasolid, stp etc) What is the procedure to achive this requirement? Where can we find the log file where its recorded that this data has been exported or imported by this user? Thanks,

Shravan

4 REPLIES

Re: NX Intellectual property logging mechanisms

Gears Phenom Gears Phenom
Gears Phenom

For what’s worth..

Are you proposing to monitor 1000+ log files?

Why not consider you own GUI & program (replicating the NX import/export capability) but one that could write the key data to a “central” log file? Probably not an easy task to do with some many users! Your internal process to import/export would then “impose” the use of your GUI/program. This is only good if one can disable the NX standard import/export options

One ought to write the workflow

 

Production: NX.CAE 9.0.3.4, NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)

Re: NX Intellectual property logging mechanisms

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The "standard" *NX* export/import functions should be able to be removed (or replaced with your code) using Menuscript.

I'm not sure how to prevent a user from "exporting" (older TC versions) or "downoading" (TC 10 or 11?) named references from TC.

 

If you are also concerned about drawings, then you have all the printing/plotting (both NX & TC) to worry about as well.

Possibly TC Visualization as well?

(there are a LOT of potential "leaks" you will have to think about)

 

Note this thread in this forum, which has code to export to DXF and STEP, which could be a starting point for your code (note I think the code listed is meant for native mode, so you'd have to modify it for TC):

 

http://community.plm.automation.siemens.com/t5/NX-Programming-Customization/Export-drawing-to-dxf/m-...

 

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: NX Intellectual property logging mechanisms

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The journal mentioned (or others like it) could also be a potential "leak". If you disable DXF export via menuscript, could a journal be run to export a DXF file anyway? I'm not 100% sure, but I think the journal would still work.

Re: NX Intellectual property logging mechanisms

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Through the OPT file of the FlexNET license server, you could include certain users using the translator licenses exclusively. This will work for any case of using the translators, batch, journal, start-menu and NX session.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide