Cancel
Showing results for 
Search instead for 
Did you mean: 

NX Journal to add attribute Part Number inside model copying file name of part

Experimenter
Experimenter

I have requirement to add multiple attributes to NX Models/Assembly. Attributes are like Description, Part number.

 

Part Number attribute value is same as OS File Name (without .prt). Do anybody has journal which can be run for an assembly and it will  put Part Name Attribute = File Name, in all child part (all level)?

 

NX Version 8.5

OS: Win7 Enterprise

 

Abhay Bhoir

+91-22-67054138

2 REPLIES

Re: NX Journal to add attribute Part Number inside model copying file name of part

Gears Phenom Gears Phenom
Gears Phenom

I got this from GTAC, which takes the OS name, and creates the attribute for the db_part_name (we use Teamcenter).  I'm sure it can be adjusted, as you need.  When you run it, it does it to every file in the directory.

 

-Dave
NX 11 | Teamcenter 11 | Windows 8.1

Re: NX Journal to add attribute Part Number inside model copying file name of part

Experimenter
Experimenter

Thanks a lot Mr DEV. It saved my time.