Cancel
Showing results for 
Search instead for 
Did you mean: 

NX Open API: UFSession.Part.CloseAll throws exception

Experimenter
Experimenter

I am using NX Open API to read information from NX files.

 

Following are steps of my code -

1. In load options, set load options as below-

    LoadOptions.UsePartialLoading = true;

    LoadOptions.SetInterpartData(false, LoadOptions.Parent.Partial)

 

2. Use "TheUFsession.Part.Open" API to open the file

3. Extract properties

4. Change load options as below -

    LoadOptions.UsePartialLoading = false;

    LoadOptions.SetInterpartData(true, LoadOptions.Parent.Immediate)

5. Use "TheUFsession.Wave.LoadParents" option to load wave relation data

6. Get Wave relations

7. Use TheUFsession.Part.CloseAll() to close all files

 

In case of some files, at step 7, an exception is thrown. The exception message is - "Duplicate Section cut found in section-cut list" or "An illegal file was given to the tag system"

 

Could anyone please guide why this is throwing exception?

 

Thanks in advance.

 

 

2 REPLIES

Re: NX Open API: UFSession.Part.CloseAll throws exception

Ken_A 1st Gear
1st Gear

See if the same error happens if you do the same steps interactively.

We've had issues with assemblies that "close all" would fail.  Only option was to Exit NX.

If it fails interactively, API won't fix that - you need to fix the assembly.

 

Also - what version of NX?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP5 + patch/TC11.2
Apparently I've turned into a gearhead


Re: NX Open API: UFSession.Part.CloseAll throws exception

Experimenter
Experimenter

Sorry,for late reply. The files are opening fine in interactive way. I am using NX 8.5.0.23.

 

The same file does not give any error if I use UFSession.Part.Close and then use UFSession.Part.Open to open the file.

 

I am trying with NXOpen.Part.ComponentAssembly.OpenComponents API now. Will update here later.

 

Thanks.