cancel
Showing results for 
Search instead for 
Did you mean: 

NX Open customization

Experimenter
Experimenter

I am trying to create a visual studio project for NXopen customization.

Here are the following steps that I tried.

1. Launched Visual Studio 2012.

2. File->New->Project

   (New Project Wizard gets opened)

3. Selected "NX10 NXOpen C++ Wizard". Used the default project and solution name and pressed OK.

4. In Application Settings, clicked on "An internal application that can be activated from an NX session (DLL)".

5. Checked on the "Explicitly (ufusr)" option and click on Finish.

6. Ideally the project should get created, but I am seeing the New Project Wizard still opened.

Do you also see the same thing?

1 REPLY

Re: NX Open customization

Siemens Phenom Siemens Phenom
Siemens Phenom

 

I just tested this with the settings you listed, and my project was created successfully.  I am testing with phase 16.