Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: NX Open with Visual Studio 2017 Professional

Experimenter
Experimenter

@DerSimulant@JimB,hello guys!

just like you do copy the vs files to vs2017 foloder, then open vs2017,could see the wizard, but it not using, says class i s not register, no CLSID object........is there any thing to do I forgot?

please help!

thanks all!vs2017.PNG

Re: NX Open with Visual Studio 2017 Professional

Creator
Creator

Hello @Tryx,

 

my problem (in those days) was that I did not see the template in my VisualStudio 2017 (all examples were obsolete).

But you can see the template, so this step works and is ok, right?

 

But If you want to create a new template, you get errors? More details please.

 

Please see my workflow:

 

1.) Create Template

Unbenannt.png

 

2.) Then this wizard starts...

222.png

 

 

Does this work on your machine?

If not: Then it seems that your wizard-files are broken or some settings are wrong.

 

 

With the help of @JimB I found my error.

@Tryx: did you check my solution here?

 

Maybe you find the bug in your setup with these screenshots.

 

regards

derSimulant

 

Re: NX Open with Visual Studio 2017 Professional

Creator
Creator

One last comment to all this stuff:

OpenNX is the wrong description. There are at least 3 kinds of licences. What I mean: It is not "open".

Quite everything is behind a paywall.

 

I have one advice to all high-level developers: Start with journals.

I just refer to the admin: Learn to use Journal files

Re: NX Open with Visual Studio 2017 Professional

Creator
Creator

FYI - I tried the same thing a few NX versions ago (NX8.5?). I upgraded ALL our NX programs to 8.5 (we have a bunch) in the latest Visual Studio. Seemed to work fine.... until some programs would randomly crash NX! When walking it through the debugger, the crash would occur when a method was returning.

GTAC and I finally realized I should have used the certified version of Visual Studio. 

We wasted a lot of time recompiling yet again.