Cancel
Showing results for 
Search instead for 
Did you mean: 

NX Plotter Configuration Directory not being stored

Pioneer
Pioneer

I've setup the NX plotter many times on many computers.  This time however, after creating or modifying an existing file and leaving the printer administration utility it forgets the directory that I pointed it to.  The files were created or modified, but it does not remember to look to that spot.  As a result, when I go to plot my only output options are image files.

WIN 7 64-BIT
NX9.0.3.4