Cancel
Showing results for 
Search instead for 
Did you mean: 

NX can't close unless the part file is closed

Hello,

 

I have launched a dialog via my application. In this dialog, I called up another dialog. When I close the second dialog via OK/Cancel, it returns to the first dialog. Then I click Ok/Cancel. The first dialog will close as well. 

 

What has been an issue is that after all these, I can't close NX unless I close the current part document first.

 

Is there anyone know the solution?

 

Thanks in advance.

 

Steph

1 REPLY

Re: NX can't close unless the part file is closed

Esteemed Contributor
Esteemed Contributor

Have you looked in the NX log file?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled