Cancel
Showing results for 
Search instead for 
Did you mean: 

NX custom for NX12 (Beta)

Creator
Creator

version.png

Hi All,

I recently participated in teh NX12 Beta testing. For further testing (event has ended) I wanted to use the NX110custom files.
I replaced all instances of "NX110" in all files and also added below line to the version declarations.

if %NX_NUMBER%==NX120 set NX_VERSION=V30.0

However, when I trie to start NX12 using the changed Custom files I get below error.

-version= - Version number should start with upper case V. eg, -version=V18.0

 

 

As you see in above code piece it is clearly written with an upper case V.
What could be the cause of the error?

Ronald van den Broek
Senior Application Engineer
Winterthur Gas & Diesel Ltd
5 REPLIES

Re: NX custom for NX12 (Beta)

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I just tried it and made no change, except edit the NX110common.bat by adding the V30 and commenting out the V29 (see image).

 

2017-05-04_10-36-41.jpg

Anthony Galante, Senior Support Engineer
PhoenxPLM
24 versions of NX installed: NX4 to NX12, plus TC11.2

Re: NX custom for NX12 (Beta)

Creator
Creator

Same for me. Works with just that change.
As soon as I change the NX_Number to 120 (and change the Library folder name) it starts complaining about the Upper case problem.

Ronald van den Broek
Senior Application Engineer
Winterthur Gas & Diesel Ltd

Re: NX custom for NX12 (Beta)

Esteemed Contributor
Esteemed Contributor

Check where NX_NUMBER comes from and change that source to result in NX120 too.

Changing this will make things work with the correct version string.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.0, FBM, MRL 3.1.4 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 10.1
Development: VB.NET, Tcl/Tk    Testing: NX12.0

How to Get the Most from Your Signature in the Community

Re: NX custom for NX12 (Beta)

Esteemed Contributor
Esteemed Contributor

It could be that for beta, they haven't changed the registry setting "version" yet?

Look in (regedit) for the keys under

HKEY_LOCAL_MACHINE\SOFTWARE\Unigraphics Solutions\NX

Is there a separate key for "12.0"?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP5 + patch/TC11.2
I'd rather be e-steemed than e-diseaseled


Re: NX custom for NX12 (Beta)

Creator
Creator

Seems to be a network issue. If I start the bat file from a mapped network drive I have the issue. If I copy the folder to a local drive then it works... Smiley Frustrated

 

Running NX11 with the same files is no issue from mapped network drive.

Ronald van den Broek
Senior Application Engineer
Winterthur Gas & Diesel Ltd