cancel
Showing results for 
Search instead for 
Did you mean: 

NX file to AutoCAD file Export in not perfect! Need Solution.

Valued Contributor
Valued Contributor

Hello All,

I tried exporting NX sheet to .dwg file. I faced few conversion error in it.

 

1. If the dimension present in the sheet is cylindrical dimension it gets converted as BLOCK Reference in a .dwg file.

2. If dimension text is overwritten the overwritten text in .dwg file comes in a wrong manner.

3. The conversion works successfully only when the dimension is set as a vertical or a horizontal dimension.

 

Please let me know what we can do for it.

 

Regards,

Abhi

2 REPLIES

Re: NX file to AutoCAD file Export in not perfect! Need Solution.

Siemens Phenom Siemens Phenom
Siemens Phenom

 

Abhi,

 

You might want to post this question in the NX Design forum.  I think it is more likely that the translator experts will see it there.

 

Best regards,

 

Steve

 

Re: NX file to AutoCAD file Export in not perfect! Need Solution.

Valued Contributor
Valued Contributor
Okay, Steve. Thanks for the suggestion.

Regards,

Abhi