Cancel
Showing results for 
Search instead for 
Did you mean: 

NX viewer, with Teamcenter?

Gears Phenom Gears Phenom
Gears Phenom

Can it be setup with NX custom, so that users that only need to view files, can use the NX viewer with teamcneter, instead of full NX?

 

Would it take a custom start_nxmanager.bat for just these users?

-Dave
NX 11 | Teamcenter 11 | Windows 8.1
2 REPLIES

Re: NX viewer, with Teamcenter?

Siemens Phenom Siemens Phenom
Siemens Phenom

NX is ultimately started by running ugraf.exe.

 

NX viewer is started by specifying the view argument to ugraf, i.e. "ugraf.exe -view"

 

Whatever .bat files are being used to start NX would need to be modified to specify the -view option

 

See Command Line Startup Switches for Windows in the online help.

Re: NX viewer, with Teamcenter?

Legend
Legend

Here's a part of a start_nxmanager.bat where users can choose if they want NX or NxViewer

 

 

echo.
echo.Please choose between NX and NX-Viewer.
echo.After 10 seconds, NX will start automatically.
echo.1. NX
Echo.2. NX Viewer
c:\windows\System32\choice.exe /c:12 /T 10 /D 1
if errorlevel 2 goto :Viewer
if errorlevel 1 goto :NX
goto :ENDOFFILE

:Viewer
%UGII_ROOT_DIR%\ugs_router -ugm -enable_cancel -version=V27 %* -opts -view 
goto :ENDOFFILE
:NX
%UGII_ROOT_DIR%\ugs_router -ugm -enable_cancel -version=V27 %* -opts -nx
goto :ENDOFFILE