cancel
Showing results for 
Search instead for 
Did you mean: 

NX10 Linux crash

Experimenter
Experimenter

Hello I have Ubuntu Linux willy , kernel 4.4 , amd64 , 8Gb of RAM

I stumbled on this accidental crash , i cannot reproduce it , i started to draw a part and while arranging some windows , NX freezed and after a while crashed(in the meantime i was clicking on menus without succes).

I will try harder to reproduce it , if i will succeed then i will post here the steps.

 

Console output error:

 

$ /usr/ugs100/bin/ugmenu
Executing ugmenux...

^C*** ERROR system never initialised, sending output to stderr ***
*** EXCEPTION: O/S ERROR: signal 2 in line 2332 of /plm/cynas/ipbuild/ugnx100/build/sandbox/src/syss/error/ind/error.cxx at Thu Dec 17 15:41:39 2015 PST
+++ General Fault Exception
[ 0] 7fa785a3b38b near UGS::Error::Exception:Smiley TonguerintTracebackToLog()+0x93 (libsyss.so)
[ 1] 7fa785a3b3f2 near UGS::Error::Exception::doTraceback(bool) const+0x2e (libsyss.so)
[ 2] 7fa7859f5e29 near UGS::Error:Smiley Frustratedignal:Smiley Frustratedignal(char const*, int, int, char const*, __va_list_tag*)+0x3f (libsyss.so)
[ 3] 7fa7859f5e60 near UGS::Error:Smiley Frustratedignal::raise(char const*, int, int, char const*, __va_list_tag*)+0x1a (libsyss.so)
[ 4] 7fa7859f6064 near UGS::Error:Smiley Frustratedignal::raise(char const*, int, int, char const*, ...)+0x80 (libsyss.so)
[ 5] 7fa7858fd19e near general_fault_handler(int)+0x167 (libsyss.so)
[ 6] 7fa783d372f0 -- signal -- (libc.so.6)
[ 7] 7fa783dfd8c0 near __poll+0x10 (libc.so.6)
[ 8] 7fa78447af72 near _XtWaitForSomething+0x472 (libXt.so.6)
====================================================
Failed to handle error condition correctly - exiting
General Fault Exception
====================================================
*** COLLAPSE:: in line 1353 of /plm/cynas/ipbuild/ugnx100/build/sandbox/src/syss/error/ind/error.cxx at Thu Dec 17 15:41:39 2015 PST
+++ Terminating due to uncaught exception
[ 0] 7fa785a3b38b near UGS::Error::Exception:Smiley TonguerintTracebackToLog()+0x93 (libsyss.so)
[ 1] 7fa7858fc527 near ERROR_vcollapse(char const*, int, char const*, __va_list_tag*)+0xf0 (libsyss.so)
[ 2] 7fa7858fc629 near ERROR_collapse(char const*, int, char const*, ...)+0x83 (libsyss.so)
[ 3] 7fa7858fd2ce near uncaught_handler()+0xc1 (libsyss.so)
[ 4] 7fa7841599c6 (libstdc++.so.6)
[ 5] 7fa784159a11 near std::terminate()+0x11 (libstdc++.so.6)
[ 6] 7fa784159c29 near __cxa_throw+0x69 (libstdc++.so.6)
[ 7] 7fa7859f5f95 near UGS::Error:Smiley Frustratedignal::doThrow() const+0x3f (libsyss.so)
[ 8] 7fa785a3ab2a near UGS::Error::Exception::throwException() const+0xd2 (libsyss.so)
[ 9] 7fa7859f5e68 near UGS::Error:Smiley Frustratedignal::raise(char const*, int, int, char const*, __va_list_tag*)+0x22 (libsyss.so)
[10] 7fa7859f6064 near UGS::Error:Smiley Frustratedignal::raise(char const*, int, int, char const*, ...)+0x80 (libsyss.so)
[11] 7fa7858fd19e near general_fault_handler(int)+0x167 (libsyss.so)
[12] 7fa783d372f0 -- signal -- (libc.so.6)
[13] 7fa783dfd8c0 near __poll+0x10 (libc.so.6)
[14] 7fa78447af72 near _XtWaitForSomething+0x472 (libXt.so.6)
====================
Fatal error detected
====================

1 REPLY

Re: NX10 Linux crash

Siemens Phenom Siemens Phenom
Siemens Phenom

 

The first thing to try would be running NX from a supported version of the OS.  NX10 is supported on RedHat Linux 6 and 7, and also SuSE Linux 11 and 12.