Cancel
Showing results for 
Search instead for 
Did you mean: 

NX10 Toolbar Customization

Genius
Genius

Working on transitioning from NX8.5 to NX10.

 

I customized the Modeling toolbar.  I added several new TABS, however one of the TABS that I customized was the default "Home" tab.  Everything is now saved under a new Role called "T10".

 

I would like to somehow get this toolbar renamed to something else, let's say "TAB5" and add the original HOME toolbar that Modeling toolbar too.

 

I figured I could copy all the code for the original HOME Tab from the ADVANCED Role and rename my HOME role to T10, but I am gettting lost in the maze of code in mtx files.

 

Could someone please help me with this?

 

Thank you,

Jerry

NX8.5 / NX10.0  Native Mode

2 REPLIES

Re: NX10 Toolbar Customization

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Rather than trying to edit .mtx files, I would suggest using MenuScript to do these customizations.

Re: NX10 Toolbar Customization

If you want to maintain this, or make it portable, I agee I would do it with files instead of roles. SFB-NX-7793  on the reitrement of the toolbar interface had a link to an excelent document NX Ribbon Customization and Transition

Mark Rief
Retired Siemens