Cancel
Showing results for 
Search instead for 
Did you mean: 

NX10 dicumentation .Net API Reference

Experimenter
Experimenter

looking to the NX10 - NXOpen Help, shows always the NX9 NXOpen .NET API Reference. Smiley Frustrated
Java and Python are up to date.

I'm using this link: https://docs.plm.automation.siemens.com/tdoc/nx/10/nx_api/

 

12 REPLIES 12

Re: NX10 dicumentation .Net API Reference

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

NX10 shipped with the NX 9 API (.net) reference; it has since been corrected in one of the maintenance releases. I guess the online docs have not been updated to match.

Re: NX10 dicumentation .Net API Reference

Siemens Phenom Siemens Phenom
Siemens Phenom

Re: NX10 dicumentation .Net API Reference

Experimenter
Experimenter
Thanks a lot ! Great :-)

Re: NX10 dicumentation .Net API Reference

Valued Contributor
Valued Contributor

Hello Jim,

 

I have downloaded the reference from the link you offered. But when I opened it, nothing is shown on the right hand side of the window. 

 

Thanks,

Kai

Re: NX10 dicumentation .Net API Reference

Siemens Phenom Siemens Phenom
Siemens Phenom

 

First be sure it is on a local drive, NOT a mapped drive.

 

Find the .CHM file in a Windows Explorer window.  MB3 -> Properties.

 

At the bottom of the properties window, does it say that this file is blocked because you downloaded it from the internet?  If so, follow the directions to unblock it.

Re: NX10 dicumentation .Net API Reference

Valued Contributor
Valued Contributor

Hello Steve,

 

The property looks like this: (coulnd't find the block information)

Property.PNG

 

Thanks,

Kai

Re: NX10 dicumentation .Net API Reference

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You "blacked" it out, but is the location on your C:\ drive?

 

Note (quite a while ago) Microsoft "broke" .CHM files if they are on a network drive or UNC path.

 

They *MUST* be in C:\  (or if you have multiple disks / partitions *ON YOUR PC*, you can put it in one of those).

 

Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: NX10 dicumentation .Net API Reference

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You can enable CHM files stored on a server share by setting the following registry key.

 

The DOS command is as follows:

REG ADD "HKLM\SOFTWARE\Microsoft\HTMLHelp\1.x\ItssRestrictions" /v "MaxAllowedZone" /t REG_DWORD /d "0x1" /f

This enables CHM files for the intranet zone.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: NX10 dicumentation .Net API Reference

Pioneer
Pioneer
Hi Stefan,
I ran the DOS command that you posted and it fixed the issue but it also broke some functionality in my Chrome Browser. How can I undo or reset these settings back to the way they were?

Thanks,
Duane