Cancel
Showing results for 
Search instead for 
Did you mean: 

NX10 instalation license server issue (windows 10)

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Good morning,

I have strange problem while installing SPLMlicenseServer v6.4.2_win64_setup (download from GTAC page). Look at attachment please - while insttallation I recived an error about some problems with loading Java VM... I have Windows 10 - 64 bit with dedicated java 8.0 version.

Trying to reinstal Java - unfortunately without positive results Smiley Sad

 

Do any of You know how to handle with this problem ? ?

========================================
Engineering >> NX10.0 Performance in the making
16 REPLIES

Re: NX10 instalation license server issue (windows 10)

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Ok problem solved. I create a new system variable _JAVA_OPTIONS=Xmx512M.

Now Java VM is loading properly. Topic for close.

========================================
Engineering >> NX10.0 Performance in the making

Re: NX10 instalation license server issue (windows 10)

Phenom
Phenom

Try installing the latest version license service (I think it's 7.2.0) that you can download from GTAC.
I am using Windows 10 and the license service (latest version) works with no trouble at all.

https://download.industrysoftware.automation.siemens.com/siemens_plm_licensing/Installs/

Thank you...

Using NX 11 / RuleDesigner PDM

Re: NX10 instalation license server issue (windows 10)

Phenom
Phenom

If my suggestion doesn't work, try to downgrade your java version from 8u60 to 8u51.

After license server is installed, you can upgrade to the last java version.

Thank you...

Using NX 11 / RuleDesigner PDM

Re: NX10 instalation license server issue (windows 10)

Phenom
Phenom
https://solutions.industrysoftware.automation.siemens.com/view.php?si=001-7481384

Problems with installing the license server for NX 10
Symptom

---------------
The 7.2.0 install will not launch on servers having Java 8 Update 60
installed.

Error: "Windows error 2 occurred while loading the Java VM"

Hardware/Software Configuration

NX

Solution

The workaround is to run one of the following commands from an
Administrator CMD window (the quotation marks are mandatory):

SPLMLicenseServer_v7.2.0_win64_setup LAX_VM "<full path to java.exe>"

--- if user has installed Java in a custom location.

or if using the default Java location:

SPLMLicenseServer_v7.2.0_win64_setup LAX_VM "C:\Program
Files\Java\jre1.8.0_60\bin\java.exe"
Thank you...

Using NX 11 / RuleDesigner PDM

Re: NX10 instalation license server issue (windows 10)

Experimenter
Experimenter

I did all of the above and none of them work

Re: NX10 instalation license server issue (windows 10)

Esteemed Contributor
Esteemed Contributor

If none of the above work, I would suggest contacting GTAC

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP5 + patch/TC11.2
I'd rather be e-steemed than e-diseaseled


Solved - Re: NX10 instalation license server issue (windows 10)

Experimenter
Experimenter

I solved this problem myself. Here is the deal. Unigraphics NX, Catia and SolidWorks installations on Windows 10 will not work with the new release of Java (Java 8 release 60). If you have that installed you must uninstall it and then install Java release 7 update 51. This resolves the issues and we are back in happy land. Now just a heads up, when you go to Java they will route you everywhere except where you need to go. They also try to get you to pay a fee for live chat. Forget that. Also do not install Java from a third party or they will wreck your computer with viruses and such. Go here to get it while you can: http://www.oracle.com/technetwork/java/javase/downloads/java-archive-downloads-javase7-521261.html#j... That is a link to the real site with the real stuff. You will have to login to Oracle or create a new login but no fees. You want to get:

Java SE Runtime Environment 7u51

It is on that page I gave the link to above.

Re: Solved - Re: NX10 instalation license server issue (windows 10)

Experimenter
Experimenter
yes.. it works thank you so much

Re: Solved - Re: NX10 instalation license server issue (windows 10)

Experimenter
Experimenter
Thank you so much, It was as you described