Cancel
Showing results for 
Search instead for 
Did you mean: 

NX10 license error license server system does not support this feature -18

Pioneer
Pioneer

Hi, Guys

Today I start to run impeller sample part in mutiple blade opertion of NX10. But I got error message "NX10 license error license server system does not support this feature -18".

 

Someone know this error before?

 

Thanks!

Canateda

-----------------------------------------
UG3.0
UG6.0
NX10.0.35
NX11.0.1
UG_NX is my favorite !!!!!!
3 REPLIES

Re: NX10 license error license server system does not support this feature -18

Honored Contributor
Honored Contributor

That error code means that NX can't currently access a license for the command that you were trying to run. For example, let's assume that the company has a single CAE license and I'm currently using it for an analysis; when you try to open the CAE application on your computer, that's the message that you would get. Your computer reqeusts the license from the server but is denied because it is already in use.

 

Perhaps this message comes up for other reasons as well, but that is the only time I've seen it.

Re: NX10 license error license server system does not support this feature -18

Do you have a turbomachinery license?

You should be able to replay and simulate the paths, but the license is needed to generate them.

Mark Rief
Retired Siemens

Re: NX10 license error license server system does not support this feature -18

Esteemed Contributor
Esteemed Contributor

The Turbo Machinery option for NX CAM is a separate license available as add-on and included in bundle NX13440.

The error means that you don't have it licensed.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.0, FBM, MRL 3.1.4 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 10.1
Development: VB.NET, Tcl/Tk    Testing: NX12.0

How to Get the Most from Your Signature in the Community