Cancel
Showing results for 
Search instead for 
Did you mean: 

NX11 Python Indexing Dictionary and Setting Random Numbers

Creator
Creator

Hello, I would like some help with the following.  Sorry if the code semantics is not entirely correct (using a lot of pseudo code in this post)  but I hope to show what I am referring to with enough detail so I can get some help.

 

I am writing a script which cycles thru sheet bodies in the workpart. Each sheet has an attribute associated with it and so I am storing each attribute in the following dictionary:

 

listA = {}

listB = {}

k = 1;

 

for bodyObject in displayPart.Bodies

          A = bodyObject.GetUserAttribute("attribute", NXOpen.NXObject.AttributeType.String, -1) 
          A_value = A.StringValue
          listA[k] = A_value
          k = k+1;

 

So lets say that listA looks something like this now:

 

listA = ["1","5","8,"12"]

 

Now I want to associate a random number with each member of the listA and store it in a new dictionary so that I get something like this:

 

listB["1"] = 101

listB ["5"] = 303

listB["8"] = 10012

listB["12"] = 91

 

I think I may need some kind of for loop to cycle thru each ListA value and assign a new value in ListB. Something like this maybe...

 

j =  get size of listA

   for 1 thru j

   listB[" listA(j) "] = random.randit(....)

 

Do you guys have some insight that may be helpful as to how to accomplish this? Thanks in advance

 

 

1 REPLY 1
Highlighted

Re: NX11 Python Indexing Dictionary and Setting Random Numbers

Siemens Phenom Siemens Phenom
Siemens Phenom

As shown in your pseudo code, listA is a list. listB is a dictionary.

 

 

You can use list comprehension and zip to generate this simply:

 

from random import *

listA = [1,5,8,12]
listB = [randint(0,10000) for a in listA]
dictB = dict(zip(listA, listB))
            
print(listA)
print(listB)
print(dictB)

 

output:

[1, 5, 8, 12]
[5895, 23, 7465, 4147]
{1: 5895, 5: 23, 8: 7465, 12: 4147}

 

 

Note that the intermediate listB is not really needed:

from random import *

listA = [1,5,8,12]
dictB = dict(zip(listA, [randint(0,10000) for a in listA]))
            
print(listA)
print(dictB)

 

output:

[1, 5, 8, 12]
{1: 6761, 5: 3750, 8: 1403, 12: 2061}