Cancel
Showing results for 
Search instead for 
Did you mean: 

NX11 cam template in NXcustom

Gears Phenom Gears Phenom
Gears Phenom

Is there something unique with the CAE template?   We use Teamcenter, so I'm using the nxdm templates, and per the readme.txt in the NX110custom files, I placed all of them in the directory shown below.  They all showed up as tabs when you did a File, New... in NX9, but the CAE tab does not display in NX11.  Any thoughts what I may be missing?

TemplateLocation.jpg

Thanks!!

-Dave
NX 11 | Teamcenter 11 | Windows 8.1
1 REPLY

Re: NX11 cam template in NXcustom

Gears Phenom Gears Phenom
Gears Phenom

FYI, the OOTB NX11 "nxdm_ugs_cae_template.pax", but not the one we used in NX9.  I did see difference when I compared the files, not sure which difference caused it not to open in NX11, so the CAE guys are going to have to tell me what doesn't work, or needs to be adjusted.

 

-Dave
NX 11 | Teamcenter 11 | Windows 8.1