Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

NX11 getuserattributes vb.net

Creator
Creator

Hi,

I've just been upgraded from nx9 to nx11

I'm working with nxopen code in vb.net

Since the update I'm now having a problem with nxobject.getuserattributes() and nxobject.hasuserattirbute() functions

If I try and call them whilst running a nxopen .dll file I get the following type of error:

System.EntryPointNotFoundException: Unable to find an entry point named 'XJA_NXOBJECT_has_user_attribute' in DLL 'libocc'.
at NXOpen.NXObject.JA_NXOBJECT_has_user_attribute(Tag objectTag, IntPtr title, AttributeType type, Int32 index, Boolean& hasAttri
bute)
at NXOpen.NXObject.HasUserAttribute(String title, AttributeType type, Int32 index)

 

If I run the equivalent code as a jounal file it works as expected.

 

I have created a new project for my code, am using vb.net 4.5.1, with the nx11 nxopen.dll files.

 

Any ideas where I'm going wrong?

 

Many thanks,

Andrew

1 REPLY 1

Re: NX11 getuserattributes vb.net

Creator
Creator

The problem was related to me using nxopen.dll files in the wrong location.

 

They moved on my installation from the previous version, so I just added references to the first instances of them that I found whilst searching my installation directory. On my installation if I used the files stored in NX\110\NXBIN\managed it worked.