Cancel
Showing results for 
Search instead for 
Did you mean: 

NX4 window 7 64 bit

Solution Partner Builder Solution Partner Builder
Solution Partner Builder
Dear all

Now I have new computer window 7 64 bit . I want to install NX4 64 bit . Can I install NX 4 64 bit ? And how to install ?

Thank you
6 REPLIES

Re: NX4 window 7 64 bit

Siemens Phenom Siemens Phenom
Siemens Phenom

 

NX4 was released a couple of years before Windows 7, so it is unlikely that we ever certified that combination.  There is no harm in trying, but don't be surprised if they don't work together nicely.

 

Re: NX4 window 7 64 bit

Phenom
Phenom

NX 4 will run on Widows 7 64 (and even windows 8 although journals dont work becuse of .NET version)

 

For dongle licence you need latest driver from rainbow.

replace lmgrd.exe with newer version (NX5 6 etc) in installer files before installing server

 

With multi monitors there is some weirdness with scroll and zoom depending on which monitor UG is on. Best result is on primary monitor at full screen.

 

I get best results with all IE integration switched off (otherwise display freezes when moving toolbars)

 

Edit Customer Defaults Gateway->User Interface->Resource Bar Tab make "Windows" field empty.

 

In ugii_env.dat add the following:

UGII_BACKGROUND_NOPART=0
UGII_DISABLE_HELP_PAGE=1

 

and comment these lines:

# The Computer Assisted Self Teach available from the Resource Bar
#
# #if FILE ${UGII_BASE_DIR}\UGII\html_files\start_${UGII_LANG}.html
# UGII_CAST_HOME=${UGII_BASE_DIR}\UGII\html_files\start_${UGII_LANG}.html
# #else
# UGII_CAST_HOME=${UGII_BASE_DIR}\UGII\html_files\start_english.html
# #endif

 

# Background Web Page. This variable defines the HTML page that is displayed
# in the background. The default is to display Tips of the day.
#
# #if FILE ${UGII_BASE_DIR}\UGTIPS\${UGII_LANG}\background.html
# UGII_BACKGROUND_URL=${UGII_BASE_DIR}\UGTIPS\${UGII_LANG}\background.html
# #else
# UGII_BACKGROUND_URL=${UGII_BASE_DIR}\UGII\HTML_FILES\background.html
# #endif

Re: NX4 window 7 64 bit

Esteemed Contributor
Esteemed Contributor

In addition make sure to use the latest MR and MP to have all the fixes available.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.0, FBM, MRL 3.1.4 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 10.1
Development: VB.NET, Tcl/Tk    Testing: NX12.0

How to Get the Most from Your Signature in the Community

Re: NX4 window 7 64 bit

Creator
Creator

agrivas wrote:

NX 4 will run on Widows 7 64 (and even windows 8 although journals dont work becuse of .NET version)

 

NX 4 Print doesn't working. Can you help me pls?

Re: NX4 window 7 64 bit


OISU wrote:

agrivas wrote:

NX 4 will run on Widows 7 64 (and even windows 8 although journals dont work becuse of .NET version)

 

NX 4 Print doesn't working. Can you help me pls?

Is there an error message?

What is in the syslog?

Mark Rief
Retired Siemens

Re: NX4 window 7 64 bit

Creator
Creator

All about this problem i written in my post

https://community.plm.automation.siemens.com/t5/NX-Programming-Customization/NX-4-Print-doesn-t-work...

 

NX 4 Print doesn't working on windows 7 x64.

Log

 

Spoiler
4 Apr, 2017 14:33:22:BPS: SUBMIT_TIME
4 Apr, 2017 14:33:22:BPS: Job 0 Submitted
4 Apr, 2017 14:33:22:BPS: Sending bSec ...
4 Apr, 2017 14:33:22:BPS: Sending bPrintTo ...
4 Apr, 2017 14:33:22:BPS: Sending myFilename ...
4 Apr, 2017 14:33:22:BPS: Sending myModel ...
4 Apr, 2017 14:33:26:BPS: Sending myPlotter ...
4 Apr, 2017 14:33:26:BPS: Sending myProfile ...
4 Apr, 2017 14:33:26:BPS: Sending C:\Users\ADMINI~1.ID2\AppData\Local\Temp\Administrator_nx4.cgm ...
4 Apr, 2017 14:33:26:BPS: QUEUE_TIME
4 Apr, 2017 14:33:26:BPS: Job Ready to Run
4 Apr, 2017 14:35:05:BPS: Downloading logfile.txt ...