Cancel
Showing results for 
Search instead for 
Did you mean: 

NX8: OCE Colorwave 300 left margin incorrect

Experimenter
Experimenter

I am having a printing issue in NX with one of my users. We use an OCE Colorwave 300 plotter, and the files they are printing keep printing out a margin on the left that’s about 2 inches bigger than it needs to be. This margin ends up cutting the drawings off on the right side, making the plots unusable. When I use the OCE Publisher software that comes with the plotter and feed the drawings through there, the plots come out perfectly.

The plotters are configured with a GPO that points to a configuration file on one of our network shares. The file appears to be created with PrintmasterNX, a product sold by SDI Software.

This is the line I am concerned about in this file:

Oce ColorWave 300:CONNECT_NT:\\grand\cw300:5:::INCHES:::::


 
How can I fix this plot quality issue in NX8? The version of NX we use is 8.0.3.4, MP8.

 

1 REPLY

Re: NX8: OCE Colorwave 300 left margin incorrect

Experimenter
Experimenter

*bump*