Cancel
Showing results for 
Search instead for 
Did you mean: 

NX9:Assigning a button to a macro or journal?

Legend
Legend

I assume there is an easier way than my current method.

 

I edit my old .TBR file. then I find that under classic toolbars and drag it to where I want it.

 

is there an easier way?

Rob Newcomb, CAD/CNC/Simulation manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 12.0.1 / Autoform r7 /WorkNC 2018 r2
Testing:nothing.
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro
1 REPLY

Re: NX9:Assigning a button to a macro or journal?

Siemens Phenom Siemens Phenom
Siemens Phenom

If you are just doing this for yourself, you can put the UI into customization mode (click on the small down arrows at the extreme right side of the ribbon bar or menu bar, or use the <CTRL> + 1 shortcut).

 

On the Customize dialog, select New Item in the Categories list. Then left click and hold on New User Command in the Items list and drag&drop it where you want the command to appear. RMB on the new button to change the name/action/etc.

 

Note that you can also add Menus, Groups, Galleries and Drop-downs in the same manner.