Cancel
Showing results for 
Search instead for 
Did you mean: 

NX9 docs on server and Post Builder

DaveK 1st Gear
1st Gear

Currently we launch NX via a .bat file, utilizing Rob Cohon's NX_Custom setup.  In the NX90env.dat file, I have the following variables set, pointing to the help files on a network server, and everything works fine from NX.

 

UGII_UGDOC_BASE_DIR=
UGII_UGDOC=
UGII_HTML_UGDOC=
UGII_CSHELP_MAPS=
UGII_CSHELP_DOCS=
UGII_CSHELP_HTML_MAPS=
UGII_CSHELP_HTML_DOCS=

 The problem is when our CAM users are running Post Builder, the help does not work, I suspected it was due to the env variables not being set, because of how Post Builder is launched, so I manually set all the variables on his machine.  No luck.  We can get it to partially work, if we install the help doc's on his local machine, and by "partially", I mean you can bring up help, but F1 doesn't bring you to the section in question...maybe this isn't an option when in Post Builder?

 

Thougths?

 

-Dave

-Dave
NX 11 | Teamcenter 11 | Windows 8.1
1 REPLY

Re: NX9 docs on server and Post Builder

I believe F1 in Post Builder brings up the Post Builder section of the help - not a specific topic.

 

Mark Rief
Retired Siemens