Cancel
Showing results for 
Search instead for 
Did you mean: 

NXOpen Alert Dialog Box

Experimenter
Experimenter

Anyone find a way of creating the Alert dialog box through the NXOpen API?

An example: Open the Edge Blend dialog and enter a value of 0.0 in the radius input box. An Alert dialog will appear informing the user of an invalid value. I would like to implement the same solution programatically.

 

Thanks!

5 REPLIES

Re: NXOpen Alert Dialog Box

Siemens Phenom Siemens Phenom
Siemens Phenom

These are not currently exposed through the NX Open API. You can use a NXMessageBox, but these do require user action to cancel.

 

You can contact GTAC to file an enhancement request to expose alert box functionality in the API.

Re: NXOpen Alert Dialog Box

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If you use a block styler dialog and specify limits for the entry box, you will get this alert box automatically.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: NXOpen Alert Dialog Box

Experimenter
Experimenter

Thanks for the reply. I wanted to verify with the community before moving forward on the request.

Re: NXOpen Alert Dialog Box

Experimenter
Experimenter
Thanks, Stefan. I was interested in using an Alert to provide feedback on a String. My assumption is that limits only work for doubles, ints, etc?

Re: NXOpen Alert Dialog Box

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The string block has only a length limit, so I think you do not like to check length of the string.

 

The string block can have the list type, so the user can only select from a given set of options.

You can set the list content at runtime, if it is depending on the part file.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide