Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

NXOpen.NXException: Matrix is non orthonormal

Creator
Creator

I am trying to practice "getting started with NXOpen 12". I am trying to recreate the examples provided with python instead of VB because I'll use python for a academic project I am trying to build. I am having following problem. Any suggestion will be helpful. thanks. Capture3.PNG

2 REPLIES 2

Re: NXOpen.NXException: Matrix is non orthonormal

Siemens Phenom Siemens Phenom
Siemens Phenom

You call the method with the X axis as both vector inputs so the error is correct.

 

PS: It would be better to post the code instead of a screenshot showing it because no one wants to write it down for testing.

See also Preserving code snippets in posts pinned down on top of this forum.

Re: NXOpen.NXException: Matrix is non orthonormal

Creator
Creator

Thanks a lot. I should be more careful of this mistakes as beginner.