Cancel
Showing results for 
Search instead for 
Did you mean: 

NXOpen - Setting font in UFTabnot

Creator
Creator

I'm automating a drawing that has very specific standards, including a specific font. It has several tabular notes. The CellPrefs.text_font attribute takes an integer input. Any ideas on how to get it to use a specific named font? Woudl I have to do it through WorkPart.Fonts somehow? Thanks!

1 REPLY

Re: NXOpen - Setting font in UFTabnot

Honored Contributor
Honored Contributor

"Would I have to do it through WorkPart.Fonts somehow?"

 

Yes, add the font to the font collection. If the font is already referenced in the part file, the NX font index will be returned. If the font is not already referenced in the part file, it will add a reference and return the NX font index.

 

The below snippet is adding the "Arial" font; after this line is executed, the value of the fntArial variable will be the NX font index.

 

        'find/assign font number
        Dim fntArial As Integer = workPart.Fonts.AddFont("Arial", FontCollection.Type.Standard)