Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

NXcustom for NX10.0 (NX100custom)

Siemens Legend Siemens Legend
Siemens Legend

Hello All,

 

Please find attached, the NXcustom for NX10.0 Revision A.

 

Also i want to use this opportunity to thank Rob Cohon for creating the foundation on which this release is based.

 

If there are any ideas for improvements, please feel free to contact me.

 

Regards,

Gerrit Koelewijn
55 REPLIES

Re: NXcustom for NX10.0

Legend
Legend
Thank you Sir!
Rob Newcomb, CAD/CNC/Simulation manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 11.0.2.7 / Autoform r7 /WorkNC 2017 r2
Testing:NX12.0.1.
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro K2200 on Win10 Pro

Re: NXcustom for NX10.0

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

First, thank you Gerrit for stepping up and taking command of a critical piece of administration.

 

In TcNX100TCIN.bat [Line 72] please comment out by default:

set UGII_UGMGR_ITEMID_IS_OSFILE_NAME=1

 

If the env var is set to anything, then exported parts will use the ItemID as their name without the RevID. I think most folks would like to include the RevID in the OS filename.

 

The value is already commented out in:

  • Tc_NX100Manager.bat [line 39]
  • NX100library\NX100env.dat [line 161]

 

Best,

/Randy


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: NXcustom for NX10.0

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

Before all thank you for your effort.

 

I found that this version saves the load_option.def file in the root of directory

In my case the path is K:\NX100custom

 

If I remember correctly past versions saves the same file in path like this:

K:\NX100custom\NX100library\CustomerDefaults\Users\username\load_option.def

 

Could this feature be restored?

 

In the first case all we user of the same office write load_option.def each other

In the second case anyone had its own on the rigth user folder

 

(I have double checked this. In NX7.5 the load_option file is saved as per second case)

 

Thank you

Fabio
I use NX10 with Gerrit Koelewijn configuration utilities. Thanks to Rob Cohon.

Re: NXcustom for NX10.0

Siemens Legend Siemens Legend
Siemens Legend

Hello Randy,

 

Thank you for the feedback!

I will put this in my next release.

 

Regards,

Gerrit Koelewijn

Re: NXcustom for NX10.0

Siemens Legend Siemens Legend
Siemens Legend

Hello Fabio,

 

The setting for the load options is still there in the NX100common.bat at line 45.

However it has been commented out already since NX8Custom_RevM

Unfortunatley I do not know the reason why Rob Cohon took this out.

It is still easy to activate when needed.

If i get more questions, i will consider to put it on by default.

 

Regards,

Gerrit Koelewijn

Re: NXcustom for NX10.0

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi Gerrit,

you can tell me the following file NX variables from the "NX100env.dat".

UGII_ALLOW_REFERENCE_SET_CSYS = 1
UGII_SECTION_USE_PLANAR_FACE = YES
UGII_DONT_CACHE_WAVE_LINK_DATA = 1
UGII_CSD_ON_DIALOG_BAR = 1
UGII_ALLOW_PMI_FLOWDOWN = 1

I can find no info
Do you have an example for me

 

Regards

 ...Christian

Re: NXcustom for NX10.0

Siemens Phenom Siemens Phenom
Siemens Phenom

 

With an appreciative tip o' the hat to Ben Broad, here is a brief description of three of those:

 

UGII_ALLOW_REFERENCE_SET_CSYS

Re-enables the ability to Create Reference Set CSYS when creating a new reference set. This functionality was removed in NX6 during a dialog redesign.

UGII_SECTION_USE_PLANAR_FACE

Prevents NX from defaulting to sketch on face when extruding from a face. See also Customer Defaults: Modeling -> Extras -> Sketch On Planar Faces.

UGII_CSD_ON_DIALOG_BAR

Used to enable class selection on the graphics display dialog bars (gwifs).

Re: NXcustom for NX10.0

Siemens Legend Siemens Legend
Siemens Legend

Hello Christian,

 

From the 2 variables leftover here the explanation.

For UGII_DONT_CACHE_WAVE_LINK_DATA :

 

   Symptom

   ---------------
   When manually breaking a WAVE link, the parent part knowledge is retained

   when using the WAVE Associativity Manager.

 

   Solution

   ---------------

   By setting the variable UGII_DONT_CACHE_WAVE_LINK_DATA = 1, NX

   will not cache WAVE specific information that can be seen when a link is broken. 

 

For UGII_ALLOW_PMI_FLOWDOWN:

 

   This is a setting that was introduced for PMI in combination with TSV (Quick

   Stack. However, this product has retired since NX8 and has been replaced

   by Technomatics VSA.

   Since this environment variable is obsolete, i will remove it in future versions.

 

Thank you for the feedback.

 

Regards,

Gerrit Koelewijn

Betreff: NXcustom for NX10.0

Valued Contributor
Valued Contributor

Hi,

 

is there a simple way to customize the location of the translator seed parts like "step214ugnullnx100_mm.prt"? I want to put them in an other dir. I don't want to overwrite them.

 

Thanks

Stefan

 

Mit freundlichen Grüßen / With kind regards

i.A. Dipl.-Ing. (FH) Stefan Walder
CAD Management
----------------------------------------------------------------------
stefan.walder@gira.de
Tel +49(0)2195-602-319, Fax +49(0)2195-91603-319
----------------------------------------------------------------------
Gira Giersiepen GmbH & Co. KG, Elektro-Installations-Systeme
Industriegebiet Mermbach, Dahlienstraße, 42477 Radevormwald, Deutschland

Intelligente Gebäudetechnik von Gira. www.gira.de

Handelsregister AG Köln HRA 16352
Persönlich haftende Gesellschafterin: GAV Management GmbH,
Handelsregister AG Köln HRB 50479
Geschäftsführer: Dipl.-Kfm. Dirk Giersiepen, Alfred A. Bulitz,
Dipl.-Kfm. Thomas Musial
----------------------------------------------------------------------
Gira Giersiepen GmbH & Co. KG, Electrical installation systems
Industriegebiet Mermbach, Dahlienstraße, 42477 Radevormwald, Germany

Intelligent building technology by Gira. www.gira.com

Register of Business Names: AG Köln HRA 16352
Partner Personally Responsible: GAV Management GmbH,
Register of Business Names: AG Köln HRB 50479
Managing Directors: Dipl.-Kfm. Dirk Giersiepen,
Dipl.-Wirtschafts-Ing. (FH) Oliver Borchmann, Alfred A. Bulitz,
Dipl.-Kfm. Thomas Musial