Cancel
Showing results for 
Search instead for 
Did you mean: 

NXcustom for NX11.0 (NX110custom)

Siemens Legend Siemens Legend
Siemens Legend

Hello All,

 

Please find attached, the NXcustom for NX11.0 Revision D.
 

There have been some changes in the architecture of NX11.0 that required specific changes in how NX is started.

The UGII_ROOT_DIR is depricated and all path's pointing to that folder from your side will need some adjustments.

 

Additionally it is now possible to deploy a predifined column configuration of the Assembly, Part and Operation Navigator.

 

More details of the changes can be found in the about.txt

 

If there are any ideas for improvements, please feel free to contact me directly by Email:

 

          Gerrit.Koelewijn@siemens.com

 

Regards,

Gerrit Koelewijn
 
Revision B has additional support for CMM Inspection.
Revision C has an added check if the NX path from the registry is correct.
Revision D contains a fix for the check on the NX location when a path contained spaces.
 
Regards,

Gerrit Koelewijn
80 REPLIES 80

Re: NXcustom for NX11.0 (NX110custom)

Siemens Legend Siemens Legend
Siemens Legend

Additional i have a question to the community.

Is there anyone who ever has decided to use the CAMauxiliary (MACH\auxiliary) folder in NXcustom?
This folder contains mostly code and has very little that can be configured. I am considering to remove this in an update.

Regards,

Gerrit Koelewijn

Re: NXcustom for NX11.0 (NX110custom)

Creator
Creator

Good question.  MACH\auxiliary used to be used for GPM/MDFG and initially for FBM.

 

Re: NXcustom for NX11.0 (NX110custom)

Pioneer
Pioneer

Hi Gerret,

 

Are there any issues transferring files from nx9 custom to nx11 custom? I would like to move all my existing customizations to the latest environment without having to recreate. Will I lose any functionality by doing so?

 

Thanks.

Re: NXcustom for NX11.0 (NX110custom)

Siemens Legend Siemens Legend
Siemens Legend

Hello nsmith,

 

It is possible to do so, but you will miss things.

An upgrade to a higher version will always require a comparison.

I usualy do the following:

  • Compare the OOTB folders and files of the old an new Version of NX
    This will tell you what has changed between the 2 versions.
  • For each difference you need to consider if merging the new functionality into your old config or or merging four changes into the new OOTB config.
    • Some folders, like CAMresource contain here and there also scripts to access libraries etc.
      unless you did extensive edits to those files i would always suggest to use the newer OOTB ones.
    • Additionally, there might be data structure changes in database files. Your data must then be updated to meet the new structure.

In general there have been changes to all the scripts that reside in the NX110custom and the NX110library.

The changes are required to support the new location for executables in NX11.

Because of de deprication of UGII_ROOT_DIR there have also been edits to the NX110env.dat file.

 

In general it is a good idea to compare everything.

 

So it is possible, but not with just a copy and paste.

 

Regards,

Gerrit Koelewijn

Re: NXcustom for NX11.0 (NX110custom)

Creator
Creator

No I don't believe I have used the CAMauxiliary folder to customize anything.

Re: NXcustom for NX11.0 (NX110custom)

Siemens Legend Siemens Legend
Siemens Legend

Hello Mark,

 

Looks like you are mistaken MACH\custom with MACH\auxiliary

 

Regards,

Gerrit Koelewijn

Re: NXcustom for NX11.0 (NX110custom)


@Gerrit wrote:

Hello Mark,

 

Looks like you are mistaken MACH\custom with MACH\auxiliary

 


Yes - I responded too quickly. I have removed the post.

Mark Rief
Retired Siemens

Re: NXcustom for NX11.0 (NX110custom)

Creator
Creator

First time user of NX110Custom. We are not using any CAM related functionality

Ronald van den Broek
Senior Application Engineer
Winterthur Gas & Diesel Ltd
Highlighted

Re: NXcustom for NX11.0 (NX110custom)

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

I am encountering inconsistent behavior between using the NX11 custom environment from a local drive and a mapped network drive. The two things I have noticed so far when the environment is on a mapped drive:

 

  1. The Menuscript "edit_ug_main.men" does not appear to run. I use a customized title that shows when I use a local environment but not one on a mapped drive.

    TITLE NX 11 - Spatial Integrated Systems, Inc.

    header_local.jpgheader_mapped.jpg

  2. The custom file templates are not used when creating a new file.

    templates_local.jpgtemplates_mapped.jpg

The setup is I have two machines, each with a out-of-the-box installa

Fred Lauzus

Sr. Application Engineer

Spatial Integrated Systems, Inc.