Cancel
Showing results for 
Search instead for 
Did you mean: 

Name of linked datums - Journal

Experimenter
Experimenter

I work on application (C#) repairing broken links. For sketches the task is quite easy - we can use following line refering to particular sketch in "source" file.

 

Sketch sketch1 = (Sketch)component1.FindObject("PARTIAL_PROTO#.Sketches|SKETCH_012");

 

However in case of datums Journal suggests to use something like that:

 

DatumPlane datumPlane1 = (DatumPlane)component1.FindObject("PARTIAL_PROTO#HANDLE R-1116818");

 

I wish to use datum's name like "centerplane" intead of R-1116818.

Is it possible to do so? I tried to use approach working for sketches (PARTIAL_PROTO#.Sketches|centerplane) , but it doesn’t work.

1 REPLY

Re: Name of linked datums - Journal

Honored Contributor
Honored Contributor

The part object has a .Datums collection that you can iterate through looking for one with a specific name. This would be one way to find a specific datum plane.