Showing results for 
Search instead for 
Did you mean: 

Native GUI from nxopen or ufunc


Is it possible to invoke a native NX GUI (for example the spline editing GUI) using nxopen on ufunc code. I have many splines in the part file. I know the tag of a particular spline. I want to invoke the spline editing GUI with the properties of that known spline tag while clicking a button. 


Re: Native GUI from nxopen or ufunc

Siemens Phenom Siemens Phenom
Siemens Phenom

In general, no, you can't launch a regular NX Open interactive process and have it take control of your session from an NX Open program.


But without a progam, you can probably double-click that spline and get the dialog you need to edit it.

Re: Native GUI from nxopen or ufunc

Esteemed Contributor
Esteemed Contributor

Not sure if this is any better than Steve's answer, but...


Would a Menuscript /PRE action program be able to "select" the spline, then call up the normal dialog?


Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled