Cancel
Showing results for 
Search instead for 
Did you mean: 

Nx 10 Plot Profile

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi, I have set a plot profile with personal customization (penprofile_1); now I need to use the same settings on another pc. Is it possible to load my profile penprofile_1, without copiyng all the settings? I cannot find information on where it is saved.

Thank youPLOT.png

 

 

4 REPLIES

Re: Nx 10 Plot Profile

Hi @Laurus,

When various preferences are set for a command dialog, it can be saved using the option 'Save Favorite As..' and the same can be loaded whenever required from the same dialog option.

Plot.PNG

 

This favorite data gets saved to a file in a local OS folder with '.fav' extension and can be located by path"C:\Users\XYZ\AppData\Local\Siemens\NX100\Favorites". From there you can copy the file and paste in the same location on another system and can be used.

 

Plot1.PNG

 

Ganesh Kadole, QA Analyst (PLM), SQS
Testing: NX 11 | NX 12 | TCIN
TC 11.2 | TC Vis 11.3 | AWC 3.2

Re: Nx 10 Plot Profile

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

The user profiles for plotting are by default stored in the file:

 

C:\Users\USERNAME\Documents\print_submit\HOSTNAME\userprofiles

 

Copy that file to the equivalent location on the other persons computer and you should be fine (as long as you have the same plotter names setup).

Anthony Galante, Senior Support Engineer
PhoenxPLM
24 versions of NX installed: NX4 to NX12, plus TC11.2

Re: Nx 10 Plot Profile

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Thank you Ganesh_Kadole, this is a good tip

Re: Nx 10 Plot Profile

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Thank you!