Cancel
Showing results for 
Search instead for 
Did you mean: 

Obsolete Resp. Sim Status - How to check this status?

Gears Phenom Gears Phenom
Gears Phenom

To all,

 

For those familiar with the Response Simulation Module in NX. If one re-runs the "attached" SOL103 Resps. Sim then the status of the Response Simulation becomes "obsolete" and one needs to do a "right-click - Check for obsolecence". 

 

I am looking for a way to check the status of a Response Simulation Solution but cannot find anything in the doc. Only how to activate one!

 

My current test code loops through all the Response Simulation Solutions (and events) and display the name to the user for selection. I'd like to display only the "valid" ones ie the ones not obsolete

 

Is there anyway of doing such check?

 

Thansk

Regards

 

Production: NX.CAE 9.0.3.4, NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)
2 REPLIES

Re: Obsolete Resp. Sim Status - How to check this status?

Siemens Phenom Siemens Phenom
Siemens Phenom

NXOpen.CAE.ResponseSimulation.Solution.CheckObsoleteStatus() will return an exception if the solution is obsolete. Invoke the method in a Try/Catch to handle it:

 

theRsManager = simPart.Simulation.ResponseSimulationManager

For Each rsSolution As CAE.ResponseSimulation.Solution In theRsManager.Solutions

    Try
        rsSolution.CheckObsoleteStatus()
        theLw.WriteLine(String.Format("Solution {0} is up to date", rsSolution.GetSolutionName))
    Catch ex As Exception
        theLw.WriteLine(String.Format("Solution {0} is obsolete", rsSolution.GetSolutionName))
        'theNXMessageBox.Show("Check Obsolete", NXMessageBox.DialogType.Error, ex.ToString)
        'Return
    End Try

Next rsSolution

Re: Obsolete Resp. Sim Status - How to check this status?

Gears Phenom Gears Phenom
Gears Phenom
Thanks a lot jimB. Much appreciated.
Production: NX.CAE 9.0.3.4, NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)