Cancel
Showing results for 
Search instead for 
Did you mean: 

Obtain hole's center (Measure Point)

Valued Contributor
Valued Contributor

Hi,

 

I'm developing on NX Open - JAVA.

How can I get the center of a hole feature?

On the UI I can do this with the "Measure Point" tool (the Journaling didn't helped me here).

 

cover.jpg

 

Thanks,

Tom.

 

5 REPLIES

Re: Obtain hole's center (Measure Point)

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

A hole feature has a .Location property that should get you this information.

Re: Obtain hole's center (Measure Point)

Valued Contributor
Valued Contributor

I tried to derive the information fron the X/Y/Z_POSITION attributes, but there is something odd:

 

The values I get from the messures are:

X = 1530 mm

Y = 1593 mm

Z = -6 mm

cover.jpg

 

But on the feature attributes I got different values:

X = -1530 mm

Y = -6 mm

Z = 1593 mm

 

cover.jpg

 

Can you please explain to me what I misunderstood.

 

Thanks.

Re: Obtain hole's center (Measure Point)

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Is this a native NX file, or has it been imported/converted from another CAD system? I ask because the native NX modeling "hole" command doesn't add attributes to the hole feature (at least not in NX 9). Is the last screenshot from the part navigator? The text "STEP2HOLE_THREAD_432" and "Recognized" leads me to believe that some other processing has happened to this file.

 

Also, are you working in the context of the piece part file or an assembly? If you are working in the context of an assembly, the measured point location won't match the attribute values if the component has been repositioned in the assembly.

Re: Obtain hole's center (Measure Point)

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

We are not speaking about modeling features, but about manufacturing features here, so these are no design features, but FBM features.

The position attributes of the FBM feature are always in relation to the start coordinate system of the feature.

I think you need to use the coordinates of the feature CSYS, which should be related to the WCS or ACS, but I haven't tested this hypothesis.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Obtain hole's center (Measure Point)

Valued Contributor
Valued Contributor

I got it:

 

private void gotIT(Face aFeatureFace)

{

   AskFaceData data = UFSession.modeling().askFaceData(aFeatureFace.tag());
   double x = data.point[0];
   double y = data.point[1];

   double z = data.point[2];

   .

   .

   .

}