Cancel
Showing results for 
Search instead for 
Did you mean: 

Obtaining beam resultants from the NX database

Valued Contributor
Valued Contributor

Hello,

 

I have a "Beam resultants - Element nodal" result. When I probe element 165 in the user interface I obtain the following result:

 

-----------------------------------------------------------------------------------------------------------------------------------
QUERY INFORMATION
-----------------------------------------------------------------------------------------------------------------------------------

Solution Name : BeamModel_fem1_sim1 : Solution 1

Load Case : Subcase - Static Loads 1
Iteration : Static Step 1
Result : Beam Resultants - Element-Nodal, Unaveraged
Units :
Force : N
Moment : N-mm
Coordinate System : Native

-----------------------------------------------------------------------------------------------------------------------------------
Elem ID : Node ID NXX MYY MZZ MXX QXY QXZ
-----------------------------------------------------------------------------------------------------------------------------------
165 : 1 3.3511E+005 -1.3253E+006 2.2955E+006 -3.3443E-008 -336.768 194.433
165 : 32 3.3511E+005 1.0079E+006 -1.7457E+006 -3.3443E-008 -336.768 194.433
-----------------------------------------------------------------------------------------------------------------------------------

 

When I use the AskElementNodalResultAllComponents, the result I get back for element 165:

 

Number of elements is: 198
The number of LoadCases in this result is: 1
Subcase - Static Loads 1
Beam Resultants - Element-Nodal
Beam Resultants - Element-Nodal
Local
Exporting subcase: Subcase - Static Loads 1 result Beam Resultants - Element-Nodal
Results for element with label: 165
NodeLabels for element:
1
32
NumComponents: 6
-1.46577250481952E+34
2.8684579564729E-42
1.52923028788504E-38
0
0
0
0
0
0
0
0
0
Axial
BendingS
BendingT
Torsion
ShearS
ShearT
Axial Force NXX
Bending Moment MYY
Bending Moment MZZ
Torsional Moment MXX
Shear Force QXY
Shear Force QXZ
-------------------------------------------------------------------------------------------
Writing results to file H:\temp\TestBeam.unv

 

 

Element 165 is defined between nodes 1 and 32 and it is a beam, so the number of components is 6. The NodalData I use in the code has a length of 12 which is what I expect (2 nodes, 6 components).

I expect the values of NodalData to be in line with the probe values, but this is not the case. I suspect that the resultParameters_Beam in the sub ExportSingle1DResultFromDatabase are not correctly set.

 

I also get different results depending whether I run it as a .dll or as a journal...

 

I have added the complete code as an attachment.

 

I hope this information is sufficient.

Regards,

Frederik

1 REPLY

Re: Obtaining beam resultants from the NX database

Valued Contributor
Valued Contributor

Hello,

 

a reply from myself which might be of help to others.

the function 'AskElementNodalResultAllComponents()' returns incorrect values and will be resolved by code changes in NX12 (PR7777757).

 

The workaround is to use the function 'AskElementNodalResult()' which works correctly and has been tested by myself.

 

Regards,

Frederik