Cancel
Showing results for 
Search instead for 
Did you mean: 

PMI dimensions export

Pioneer
Pioneer

Hi,
How can we export PMI dimensions,textnotes along with requirement numbers to excel?

 

 

Thanks & Regards,
Ravi

3 REPLIES

Re: PMI dimensions export

Siemens Creator Siemens Creator
Siemens Creator

Run the PMI report tool from NX.  You may need to modify your tool bar to add it.  What it does is pull all PMI types into the excel file with the PMI data ie qty size etc. the excel file winds up being about 132 columns.

Re: PMI dimensions export

Pioneer
Pioneer

Thanks for the info. But we need columns only as per our requirement.

Re: PMI dimensions export

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Assuming somewhere in the 132 columns is the data you need for each PMI "dimension"...

 

Write a VBA program to massage the data from NX & output as required.

Without knowing more, and assuming the NX output is a single sheet in Excel, I'd probably

- Make a new sheet

- Run thru the existing sheet row by row, massaging as required & output to a row on the new sheet

- When done processing all rows, delete the old sheet

- Save the .XLSX

 

Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled