Cancel
Showing results for 
Search instead for 
Did you mean: 

Physical Material Usage

Pioneer
Pioneer

Does anyone know of a method to determine if a PhysicalMaterial is used in the current part?

I have

Dim LocalMaterials() As PhysicalMaterial =displaypart.MaterialManager.PhysicalMaterials.GetUsedMaterials

but this returns materials that are used in components as well as displayPart. The Manage Materials window differentiates between used, un-used, and used in components as well as giving the location of the material. I just can't seem to locate a method to get this information.

4 REPLIES

Re: Physical Material Usage

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

This may not be the best or only way to do this, but here's what I came up with. It will report the materials available (locally) in the work part, it reports the material assigned to each body, and it reports which available materials are not used in the part. If you want to query an assembly, you could modify the code to process each component and report the used/unused materials in the full assembly.

 

Option Strict Off
Imports System
Imports System.Collections.Generic
Imports NXOpen
Imports NXOpen.UF
 
Module Module2
 
    Sub Main()
 
        Dim theSession As Session = Session.GetSession()
        Dim theUfSession As UFSession = UFSession.GetUFSession()
        If IsNothing(theSession.Parts.BaseWork) Then
            'active part required
            Return
        End If
 
        Dim workPart As Part = theSession.Parts.Work
        Dim lw As ListingWindow = theSession.ListingWindow
        lw.Open()
 
        Const undoMarkName As String = "report material usage"
        Dim markId1 As Session.UndoMarkId
        markId1 = theSession.SetUndoMark(Session.MarkVisibility.Visible, undoMarkName)
 
 
        Dim materialsInPart As New List(Of PhysicalMaterial)
        Dim unusedMaterialsInPart As New List(Of String)
 
        For Each tempMaterial As PhysicalMaterial In workPart.MaterialManager.PhysicalMaterials.GetUsedMaterials
            materialsInPart.Add(tempMaterial)
            unusedMaterialsInPart.Add(tempMaterial.Name)
        Next
 
        lw.WriteLine("Materials available in part")
        For Each temp As PhysicalMaterial In materialsInPart
            lw.WriteLine(temp.Name)
        Next
        lw.WriteLine("")
 
        lw.WriteLine("Bodies in part")
        For Each tempBody As Body In workPart.Bodies
 
            lw.WriteLine("body tag: " & tempBody.Tag.ToString)
 
            If tempBody.HasUserAttribute("Material", NXObject.AttributeType.String, -1) Then
                'body has a material assigned, remove it from the "unused" list
                Dim materialAttribute As NXObject.AttributeInformation
                materialAttribute = tempBody.GetUserAttribute("Material", NXObject.AttributeType.String, -1)
                unusedMaterialsInPart.Remove(materialAttribute.StringValue)
 
                lw.WriteLine("material assigned: " & materialAttribute.StringValue)
 
            Else
                lw.WriteLine("no material assigned")
            End If
 
            lw.WriteLine("")
 
        Next
        lw.WriteLine("")
 
        lw.WriteLine("Unused materials")
        For Each temp As String In unusedMaterialsInPart
            lw.WriteLine(temp)
        Next
 
        lw.Close()
 
    End Sub
 
 
    Public Function GetUnloadOption(ByVal dummy As String) As Integer
 
        'Unloads the image immediately after execution within NX
        GetUnloadOption = NXOpen.Session.LibraryUnloadOption.Immediately
 
    End Function
 
End Module

Re: Physical Material Usage

Pioneer
Pioneer
I did a similar approach to this as well. The problem I had run into is if the same material is used in both the part and the component there is not a way to differentiate between the materials in order to only delete(or reuse) the one in this part.

Re: Physical Material Usage

Valued Contributor
Valued Contributor

I use the following to determine if an assembly has materials assigned.

Dim LocalMaterials() As PhysicalMaterial =displaypart.MaterialManager.PhysicalMaterials.ToArray()

 It does not report the materials of the component parts.

Mike

NX 12.0.0 TC11.3 VMU 11.3

Re: Physical Material Usage

Pioneer
Pioneer

Thanks. This returned an array of Material, not PhysicalMaterials, but it worked for my purposes.