Cancel
Showing results for 
Search instead for 
Did you mean: 

Point to Point Drilling operation

Valued Contributor
Valued Contributor

Hey,

 

NX Cam - JAVA.

I got a Point to Point Drilling operation.

Is there a way to reach to the relevant face\s?

 

Thank you,

Tom.

4 REPLIES

Re: Point to Point Drilling operation

Esteemed Contributor
Esteemed Contributor

P2P doesn't use face information in the way drilling operations do, so I doubt there is a possibility other than checking the drill locations and search for faces around them.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.4 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 10.1
Development: VB.NET, Tcl/Tk Testing: NX12.0 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink

How to Get the Most from Your Signature in the Community

Re: Point to Point Drilling operation

Valued Contributor
Valued Contributor

Hey Stefan, Thank you for your answer.

Do you have any idea how can I do that?
How do I perform a search around a location?

Re: Point to Point Drilling operation

Esteemed Contributor
Esteemed Contributor

Sorry, never had a need to do this, so I don't know what is needed in detail.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.4 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 10.1
Development: VB.NET, Tcl/Tk Testing: NX12.0 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink

How to Get the Most from Your Signature in the Community

Re: Point to Point Drilling operation

Esteemed Contributor
Esteemed Contributor

The other issue with PTP operations is that (largely) you can only use GRIP to automate them.

Siemens has stated there are *no* plans to ever support PTP with API (beyond what is already there).

 

*IF* you can, try to use holemaking operations instead.

If you come up with limitations in holemaking (and youhave time) file IRs with GTAC, and see if your issue is a PR or an ER (Enhancement).  If the latter, you can post the ER number here so people can file "me too" ERs to increase the chance the ER will be implimented sooner (rather than later...)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled